In an effort to improve your experiences on our website we have updated our menu. Our new navigation makes it easier to find products, software, and content tailored to your industry or interest. We have also updated our contact and support section to better serve you.
See highlights from 2016's Emerson Global Users Exchange in Austin, Texas!
1:49
You want to take advantage of status & diagnostics in intelligent devices, but within a short amount of time you are inundated with alerts. Sometimes a single root cause results in a device generating five or more alerts.
47:25
3M and Emerson collaborated to improve 3M’s existing solvent delivery system. The system was migrated from an energy-intensive, pressure-based system to an on-demand system with intelligent monitoring and bookkeeping.
32:53
To measure the efficiency of a coal fired power plant, the term heat rate is commonly used. Heat rate is the measure of energy put into a system (Btu/kWh), divided by electricity generated(kW).
41:50
Traditionally capital projects only focus on the total installed costs and give no consideration to long term value and future profitability. That’s all changing. Companies want to spend their money in the smartest way possible.
36:39
There are many hazardous processes in today’s refineries which, in the event of an accident, can pose threats to human health, environment and operations. Refiners strive to make safety a top priority at their facilities, which can be seen...
36:14
We will follow case studies of Grounding Methods in Process Controlled Plants, Physics of Electrical Events and accumulative effect of low impedance AC exposure on Automation Systems. Most Power and Grounding designers believe that a traditional Grou
54:14
The UND Power Plant team set a goal to improve the performance of their DeltaV alarm system. This presentation discusses their game plan for achieving victory including the goals they wanted to achieve and the process they went through.
45:20
The Duke Buck Combined Cycle station was in need of a reliable high pressure spray attemperator isolation valve solution. This solution was required to provide bubble tight shutoff over many cycles...
22:03
After using several level measurement technologies, the Chemours LaPorte plant was unable to measure the true level of Fluorospar in their two storage silos. Fluorospar is a dusty, powder-like material used in the production of Hydrofluoric Acid.
24:00
For almost a decade, Hunt Refining Company has been a leading user of Emerson’s wireless technology. Initially, there was some resistance due to concerns of network reliability, security and integration into the existing DCS.
45:41
Abkatun-A Offshore Platform located in the Mexican Gulf installed on March 5th, 1982, was affected by a fire last April. Beside the crude compression as the main task (4 compressors), this platform manages deluge water, power feed...
41:36