New Operator Overview Dashboards
35:19
Description
Related Videos
This presentation illustrates the paradigm shift for operations personnel on changing from panel board graphical interfaces to the current Delta V System Overview Dashboards used at SRS Tritium Facility. As the operator graphic interfaces were changed over the years, a lot of resistance was met, e.g., why can't we have what we got now. The new dashboard design allows the operators to quickly scan the heartbeat of a system to determine if they need to explore further. System engineers and experienced operators were used in the development of these dashboards to capture the pertinent data.
View More
View Less