Which Are the Approved Certifications That the Updated Roxar™ Watercut Meter Benefits From?
1:06
The Roxar Watercut meter comes with the latest ATEX or IECEX approvals. ATEX is the preferred European standard, while IECEX is widely recognized internationally.
Related Videos
For "Roxar"
-
Play video What Measurement Technology Does the Roxar™ Watercut Meter Use?
What Measurement Technology Does the Roxar™ Watercut Meter Use?
The Roxar Watercut Meter is a highly sensitive, full-bore instrument using advanced microwave resonance technology. Trusted globally in demanding onshore and offshore environments, it excels in water cut measurement across various...
1:38
-
Play video Taking Autonomy and Precision of the Roxar™ 2600 Multiphase Flow Meter Into the Future
Taking Autonomy and Precision of the Roxar™ 2600 Multiphase Flow Meter Into the Future
Introducing the Roxar 5726 Multiphase Transmitter, the new electronics hardware platform for the Roxar 2600 Multiphase Flow Meter, offering high measurement resolution and processing power for improved autonomy and data analytics.
2:08
-
Play video Which Applications Can Benefit from Using a Watercut Measurement?
Which Applications Can Benefit from Using a Watercut Measurement?
From water cut measurement on the oil outlet of a three phase separator to allocation or fiscal measurement at an oil pipeline, or at a desalter inlet in a refinery, or even fiscal quality measurement at a refined pipeline, the field proven Roxar...
1:48
-
Play video Simplifying Operations with Intuitive Interface for Roxar™ 2600 Multiphase Flow Meters Enabled by the Roxar 5726 Multiphase Transmitter
Simplifying Operations with Intuitive Interface for Roxar™ 2600 Multiphase Flow Meters Enabled by the Roxar 5726 Multiphase Transmitter
Updates to the Web User Interface provide straight forward and intuitive approach to all communication needs with the Roxar 2600 Multiphase Flow Meter from Emerson.
1:53
-
Play video H2S, Sand, Scale and Wax and The Roxar 2600 Multiphase Flow Meter
H2S, Sand, Scale and Wax and The Roxar 2600 Multiphase Flow Meter
The Roxar 2600 Multiphase Flow Meter has proven to be robust and is performing well with all the various assisted recovery methods.
2:56
-
Play video What Is the Measuring Range of the Roxar™ Watercut Meter?
What Is the Measuring Range of the Roxar™ Watercut Meter?
Explore the enhanced versatility of the Roxar Watercut Meter with the TopCut feature, expanding its range from 0-50% to an impressive 0-100% water cut, perfect for applications requiring a broader range.
2:03