Emerson Navigation Clone

Flexim Flow Disturbance Correction

2:44

In the often limited space of industrial process plants, recommended straight-run requirements can be challenging to find. Due to restricted pipework, it’s not always possible to carry out the optimum installation as advised, away from valves, bends, and other inline components that could cause excessive and problematic turbulence. Clamp-on flowmeters typically require an inlet length of at least 10D for accurate measurement to be achieved. Thanks to Flexim’s disturbance correction, good accuracy is achieved even at non-ideal inflow conditions, reducing the required inlet length from 10D to just 2D. This innovation means installation is executed in even the tightest spaces without process interruption. This is undoubtedly a great benefit Flexim can provide. This video focuses on this valuable feature and how Flexim achieves flow disturbance correction. The Flow Disturbance Correction is now offered in the following meters: FLUXUS F401 FLUXUS F50 Series FLUXUS 60 Series FLUXUS 70 Series FLUXUS 72 Series FLUXUS 80 Series FLUXUS 831 PIOX S721 PIOX S831

View More
View Less
Emerson Corporate Footer

Share this video

Embed